Other Parts Discussed in Thread: UCC28700
Hi,
There are errors in the circuit. Simulation aborted
UCC28700.txt (50):
*** ERROR *** Instance 'X_U_TOP_U_SAMPLER_U62': wrong number of nodes in call to sub-circuit 'one_shot'
UCC28700.txt (489):
...
*** ERROR *** Instance 'X_U_TOP_U_MOD_UPCC_U62': wrong number of nodes in call to sub-circuit 'one_shot'
Also when I tried to change the code shown below (One_shot for two different values of T=330 or 200), the above error got resolved but a new error came.
ERROR occurred after changing the spice code as per above changes: