Other Parts Discussed in Thread: TIDA-010081, TIDA-010080
Hi experts,
In the datasheet, section 9.2.2.1, "Generally, the on-state resistance must be selected so that the 35-mV proportional gate drive threshold doesn't get activated until last 25% of the overall conduction time."
Here is my question, due to my LLC converter maximum output current is 50 A, and almost all the available MOSFET that can be chosen come with Rds_on far larger than the recommended value. So I am asking what if the Rds_on of the implemented MOSFET is far larger? And if I choose to parallel the MOSFET will Rds_on be equally divided?
Thanks