This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2678: LM2678 for supply that can switch between output two voltages

Part Number: LM2678


I want to design a power supply that can switch between 5V and 12V outputs, 4.5 amps max, 34-38V input. Looking at LM2678. Using the design information Cin, Cout, and L1 are quite different between a 5V design and a 12V design. Which do I use so that I can switch between the two output voltages (with a switch to change the resistor value)?