Hi,
The figures 50, 51 and 52 in the datasheet show a ramp up time of ~400ms where figures 53, 55 and 56 are showing a ramp up of ~400us.
There is a factor of 1000 between the two sets.
Can you confirm it is not a typo and the device ramp up time is highly impacted by the output current ?
If it is not a typo, do you have any graph to indicate the ramp up time vs the output current ?
A ramp up of 400us vs 400ms is a huge difference in a design and if our current is somewhere in between, we would like to know what the ramp time will be for any current between 0 and 200mA please.
Thanks,
Luc