This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650250: How should I handle the unused output pins on TPS650250

Part Number: TPS650250

Hi,

My customer tries to use TPS650250 by replacing from multiple power ICs.

 

They only use Vout:3.3V, 2.5V, 1.2V by DCDC1, DCDC2 and DCDC3.

Thus, they don’t use LDO1 and LDO2.

 

In this situation,

Could you answer how they should handle the unused output pins, VLDO1, VLDO2, FB_LDO1 and FB_LDO2?

Or if EN_LDO is connected to GND, don’t they have to do anything about unused output pins?