Hello team.
Customer finished the evaluation of production variant of BQ25171-Q1 - BQ25171QWDRCRQ1.
The evaluation results are the same as were received on preproduction samples ( this is completely described in initial thread).
If customer sets the charge limit to 4.2V, then charging process stops while batteries are not fully charged.
If customer increases the number of cells in BQ setup only, but leaves the same amount of cells on the board (BQ setup -1), then BQ overruns the timer and indicates an error.
So the question is:
is it possible to use BQ25171-Q1 to charge NiMH-cells completely without cheating the BQ configuration and without getting an error?
Thank you.