This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS564201: Voltage Drop

Part Number: TPS564201

Hi,

I am using TPS564201 IC. Input: 12V, Output: 5V. It's said in the datasheet, I'm using a 3.3uH coil. Model number of the coil SRP7050AA-3R3M.

When I load 1A from the 5V, there is a voltage drop of 0.5V. (output voltage 4.5~4.6V)

What is the reason?