I have a question regarding the TLV752 which is a dual output device:
Are the two outputs fully independent regarding the 'Functional Block Diagram' or do they share some circuit elements? I want to use one output for powering a microcontroller and the other output for a noise sensitive RF application, so I would prefer if the circuits of the two outputs are fully seperated.
In the datasheet there is a 'Functional Block Diagram' but only for a single output.
Thanks in advance.