For this part, if R3 (Mode/S-Conf) resistor is 118 K it will operate in mode 16 (VSET, 1MHz, no discharge, Forced PWM)
What if the resistor is larger than 118 K, will it remain in mode 16?
If yes, then I can use a standard 10% tolerance resistor > 131.1 K ( e.g. 150 Kohm)?
The part will still operate in mode 16 correct?
Regards,
Mike