This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62912: Lowest noise option for AM/FM tuner application

Part Number: TPS62912


Evaluating the use of the TPS62912 in an application where it will power an AM/FM tuner device.  application is12V => 3.3V, relatively low current ~150mA typical, 200mA max.  Considering this device due to the efficiency over a linear regulator operating over such a large voltage drop, and for low noise.  There is some concern that the switching frequency / spurious will be unsuitable in a tuner application.    Looking for recommendations for alternate devices in this application, for example I've also evaluated the TPS543620 and welcome feedback over the preferred device for the two, or other suggestions.