Hi,
1.
I wonder the current limit spec of LM34927. Datasheet specifies its threshold is 1.02Vtyp.

But it looks this threshold is for a peak value, but average value would be less than the peak value according to DS below. Does this mean current limit can be triggered even with the current in the buck switch < 1.02A?

2.
What's endurable current spec not to damage the device? Customer reported LM34927 was damaged in the EVM while supplying power to gate drivers on their board. They are looking for reason and putting a possibility that the load current was too high, so they want to check the endurable current spec of LM34927.
Thanks,