Hello,
My customer is looking to create a 200mA ±15V supply rails with 200mA load capacity from a DC24V supply. They liked the TPS54060 since it has a tracking feature but were wondering if the device can track a negative supply?
Idea would be to have a standard buck from 24V to 15V and an inverting buck boost from either +15V or +24V to -15V. The key is they want the +15V and -15V supplies track each other on power up and power down. Other parts or ideas is appreciated!
John