Other Parts Discussed in Thread: UCC28180
Hi,
I used the reference design UCC21180EVM-573 in my power supply. As the result, it failed the conductive emission at the program frequency 40 Khz with the the Rfreg of 26.1 Kohms. I have an AC line filter in the front end after AC input to pass some of the high frequencies of 163 Khz, but still have high peak of 40 Khz. I tried to program the frequency up and down from 15 to 100 Khz, but the amplitude of the frequencies don't change. Do I need to add one more external line filter? if yes, what would the values of the inductance/capacitors be? I don't have any way to sweep the frequency band. Any advise would be greatly appreciated. Thanks
Bobby.