Hello
would someone be able to clarify the drop out voltage of the TPS780330220 for me please?
I intend to use the device with an output voltage of 3.3v fixed and an input voltage of 3.6V and a load current of between 5-10mA.
I see on the data sheet that the drop out voltage is given as 200mv at 150ma. I am looking at the dropout voltage graphs and I am not clear on what drop out voltage I expect at my load current. The condition on the drop out graphs show input voltage as being 95% of output voltage which won’t be the case in my application.
could someone please confirm the drop out voltage for my application please ?
Thanks