Hi,
Now I,d like to use LM317 with adjustment resistor to produce 0~10V signal.
But the output range of LM317 is 1.25V to 37V.
The input is DC 24V.
My idea is that using buck-boost circuit produce a negative voltage,such as -2.5V.
Is there any better method?
Thanks.