This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3658: Min input voltage

Part Number: LM3658


The data sheet for the LM3658 shows a different min input voltage for the AC adapter input (4.5V) vs the USB input (4.35V). 

I assume this is because of the maximum charge current limit is different for these inputs. 1A for the AC adapter input and 500 mA for the USB input. The specified minimum input voltages would allow enough headroom to charge the battery to 4.2V. 

My customer is limiting the charge current to 200 mA but needs to support a Vin minimum of 4.3V. If we assume that the dropout resistance of the charge control FET is the same as the 4.5V and 4.35V cases, then it seems the LM2658 could support a 4.3V input and still fully charge to 4.2V, at least at t = 25C.

Is this analysis correct?