Other Parts Discussed in Thread: USB2ANY
I wrote [0xB1, 0xFE, and 0xA3] to the password register of TPS6521835 using the USB2ANY debugger tool. Coin cell was not inserted and after the write, status register showing FSEAL bit as 0b only. This issue not happening when i tried with coin cell. And another observation i found is after making FSEAL bit as 1b and then removed the coin cell and external power. After a few seconds when i again powered on the board without coin cell, FSEAL showing as 1b even without doing any register write operation.
can anyone help on this.