Other Parts Discussed in Thread: USB2ANY, TPS25750, BQ25792
Hi,
I bought USB-PD-CHG-EVM-01 and in order to program it I saw in "Order & start development" that I need USB2ANY so I bought it also.
I have seen in one video that it can be very easily programmed with the TPS25750 application customization tool but I see that it need to be connected with a COM port.
The problem is that USB2ANY appears only as HID and not as COM port.
Did I make any mistake with the connection?
I have seen the the right connection from USB2ANY to the EVM and made the right connection between them.
The USB2ANY Explorer software recognize the USB2ANY board
If I am correct I need to program the TPS25750 and it will handle the BQ25792.