Other Parts Discussed in Thread: TPSM82823,
whether the part (TPS82085 and TPSM82823)'s ripple be suppressed below 10 mV?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Depending on the mode of operation, yes it can be reduced below 10mV.
If the devices run in PSM mode (which is pulse-frequency operation) naturally the ripple will be greater than if it they are working in PWM mode.
Regards,
Davor