Other Parts Discussed in Thread: TPS92200
Hello TI-Team,
we need to power a backlight of an Display with the following specs:
Vin=24VDC
Backlight:
Vf=19,2V
If=40mA
2 LED strings á 6 LEDs
I thougt, the LM3407 might be a good choice, but i´ve read the threat title "LM3407: Repeat inductor failures with low-current operation", and now i´m not sure, if i will run into issues, using this IC.
Is there any suggestion for this driver in low current application? Is there another driver more suiteable?
Thank You
Max