Hello,
WE would like to use UCC28061 in our mainstream products as this is only controller currently available on the market .
But we found a problem. During start-up with low line voltage (90Vrms) even at very low load (5W) , the inductor current can jump (depending on which part of sinusoidal voltage the start occurs )
to extremely high level (40A and more). We found this is to be due to the input EMI filter having differential mode chokes. We tried to simulate this circuit using SIMPLIS simulation model for UCC28054, downloaded from TI. Simulation shows the same problem. Could you, please, help to solve this problem
Regards
Lev