This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3414HV: Do you have any device like external FET version of LM3414 or LM3414HV?

Part Number: LM3414HV
Other Parts Discussed in Thread: LM3414, TPS92640

 Hello guys,

 One of my customers is interested in LM3414HV. But the device output current capability is 1A.

 They want to drive 100V~150V Vf LED with higher current than 1A and 220V input.

 So they are looking for a device like external FET version of LM3414 or LM3414HV?  

 I attached the requested block diagram from the customer. 

 Do you have any device like such device?

 Or do you have any plan to develop the device?

 Your reply would be much appreciated.

 Best regards,

 Kazuya.

BlockDiagram.pdf