Other Parts Discussed in Thread: UCC12040
Hi Team,
do we have DC Insulation Curves available for the UCC12050?
Regards,
Alen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alen,
TI completes safety isolation testing at independent agencies such as UL, VDE and CQC, as well subjecting the UCC12050 and UCC12040 to our own internal isolation breakdown testing. The isolation limits given in the data sheet are verified by the safety agencies and TI and additional safety margin is added. The breakdown data is not public. Do you have a customer asking for "DC insulation curves" and can you provide an example of what the curves look like?
Regards,
Steve M
Hi Steve,
my customer is saying the projected lifetime is always based on AC voltage Do you think this value can be just calculated to DC and is valid?
Regards,
Alen
Alen,
UCC12050 is a transformer based DC/DC converter module. Projected lifetime based on DC voltage makes no sense from an isolation point of view.
Steve
Hi Steve,
there is a constant DC voltage of up to 2000V on the DC/DC, the transformer and on the isolators.
If the customer can convert AC to DC with square root of 2, this would be fine for them.
1414VAC = 2000VDC
Any thoughts or concerns?
Regards,
Alen
Alen,
I'm not so concerned the HV on just one side of the isolation boundary but what really matters is the voltage differential across the isolation. Also, no problem on the SC/DC conversion. I assume we are referring to a pure sine wave for the AC voltage?
Regsrads,
Steve M