Other Parts Discussed in Thread: TPS3813, TPS3850, TPS3851
Hi Team,
Now customer use BD87A41FVM-TR !
There is a good new that we have a chance to DIN
Do we have a solution to compete with BD87A41FVM-TR ? I need a P2P solution ,THX
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Now customer use BD87A41FVM-TR !
There is a good new that we have a chance to DIN
Do we have a solution to compete with BD87A41FVM-TR ? I need a P2P solution ,THX
The TPS3851H50SQDRBRQ1 would be the closest but it is not pin to pin and there are several differences in parameters. We can try to see if a different orderable or one of the other TI WDT supervisors like the TPS3850, TSP3852 or TPS3813 or one from the TPS382x family may be a good fit. Can you share the customer needs? If needed you can post on the internal forum or send internal email
Hi Padgaonkar Ajay ,
Could you help share the comparison table? THX
I want to use this information to discuss with clients!
https://www.mouser.tw/datasheet/2/348/bd37a19fvm-e-1874331.pdf
Hi Kygo,
See below for comparison table. I am not sure if you are aware, but we also happen to have this information publicly available, so you can conveniently gather this information yourself! For future reference, http://ti.com/svs will give you a great offering of our whole portfolio. It also has a very convenient parametric search so you can find the perfect part for your customer!
Part Number | NICHE | Function | Manufacturer | Rating | Bucket | Temp Min(°C) | Temp Max (°C) | Iq (Typ) (uA) | Iq (Max) (uA) | VCC (Min) (V) | VCC (Max) (V) | # of SuActive-Low Push-Pullies Monitored | Reset Threshold Accuracy Typ. (%) | Hysterisis Typ (%) | VPOR | Output Driver Type | Reset Output | Time Delay Typ (ms) | Watchdog Timer WDI (sec) | Package Size Min (mm2) | Package Size Max (mm2) | Package Group | Approx. Price for 1KU (US$) | Special Features | Manual Reset |
TPS3851 | PRECISION | PRECISION & WD | TI | Catalog | Watchdog | -40 | 125 | 10 | 1.6 | 6.5 | 1 | 0.8 | 0.5 | Active-low | Active-Low Open-Drain | 200 | Programmable | 9 | SON | 0.65 | Active Low Enable, Manual Reset, Watchdog Disable, Watchdog Timer | Yes | |||
BD87A41FVM | #N/A | #N/A | Rohm | Standard | Watchdog | -40 | 105 | 5 | 14 | 1 | 10 | 1 | 2.5 | 3.5 | Active-low | Active-Low Open-Drain | Programmable | Programmable | 11.6 | MSOP8 (8) | 1.31 | Watchdog Timer | No |
-Tony