Other Parts Discussed in Thread: TPSM82480, TPSM82810
I tried creating a footprint for this part but the datasheet is obviously wrong. It shows the distance between pad 1 and pad 2 is 1.45mm but when I do that the pads overlap. Please advise.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Todd,
Can you please clarify where the error is? I see a 1.45mm dimension on the land pattern drawing on page 32, but this distance is the distance from the center of pin 1 to the center of pin 2 (actually, the dimension is on pin 19 and pin 20 but it also applies to pin 1 and 2). Taking half of the 0.6mm width of pin 2 and half of the 1.7mm width of pin 1, I get 1.15mm. This leaves 0.3mm between the 2 pins.
We also offer the footprint here:
https://www.ti.com/product/TPS84410#design-development##cad-cae-symbols
Finally, why do you use this older, larger module? We have the newer, much smaller TPSM82810 and TPSM82480.
Thanks,
Chris