Hi,
Looking to power mux two 1.8V supplies to a processor to serve as primary and a back up supply, current needed it very small at 1mA max. Would like to see if TPS2116 would be a good fit here as most of the other power mux available have an VIN min that is too high. Current protection is not needed but rather what is liked is the automatic switchover when voltage sensing is too low.
Best regards,