Part Number: TPS61379-Q1
no load ,boost voltage is ok; add load ,no output;
input voltage:5V; set output voltage is 12V:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS61379-Q1
no load ,boost voltage is ok; add load ,no output;
input voltage:5V; set output voltage is 12V:

Hi Terry,
During startup, the TPS61379-Q1 starts switching and needs energy to charge the Cout to setting output voltage.
Since this device cannot startup with heavy load, please run the startup test with no load.
For the inductor value, it's recommended to use a 1uH or 1.5uH inductance for this application.