Dear Ti,
I have custom board with Bq76930 , which when put to Load cell-0 Voltage varies with 30-50mV from Actual , please some one comment here , am wondering whjy it must be happening.?
Thanks ,
Rohit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ti,
I have custom board with Bq76930 , which when put to Load cell-0 Voltage varies with 30-50mV from Actual , please some one comment here , am wondering whjy it must be happening.?
Thanks ,
Rohit
Dear Matt, please find snaps of my schematic , as am unable to find option how to attached file to this reply.
Above is Lower AFE Schematic.
Above is Upper AFE schematic.
Matt apart from Above Cell-0 Matter, i have sleep/ Shut down current of 300micro Ampere, can you please see in schematic , as how to reduce it to 1micro Ampere?
Also here am unable to share attachement of Schematic, can you please share how to share full attachment of schematic , so that you can review eaisly.
Rohit
Hi Rohit,
Maybe you can create a zip file and upload it? Also, in the title of this thread are you saying that you are connecting 10 cells (instead of 20)?
Thanks,
Matt
Dear Matt,
Yes title is for 10 cells ,but actually my project is for 20S.
Please find attached pdf file for AFE section, Please look in to it for Cell-0 deviation from actual value while charge or discharge.
Hi Rohit,
Since you say the deviation occurs while charging or discharging, I suspect there is an interconnect resistance between the bottom of Cell0 and the board, so you are seeing an IR drop when current is flowing.
Regards,
Matt