Other Parts Discussed in Thread: BQ24314,
Hi
I'm currently working on a project using the BQ24314.
The input voltage comes from a USBC interface, and given that the USBC standard has been updated to support higher power/voltage (240W/48V), I need to replace the component with a similar component that would be able to support and protect against a higher voltage.
We're still using 5V as input to our system, but want to protect against possible faults.
Grateful for any help in finding the right component.
Regards