This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2621: LM2621 in/out voltage

Part Number: LM2621
Other Parts Discussed in Thread: TLV61046A

Hi team, 

I have a project use LM2621 create 10V from 3.3V , the load current about 40mA. As show below Schematic 1 and Schematic 2

-> with input voltage is 3.3V, have any problem to generate 10V at the output?

-> In the Schematic 1,I think  the EN(2 pin), VDD(6 pin) pins are overvoltage

 

Best Regards !