Other Parts Discussed in Thread: TPS62122, , TPS62901, LM2621
Hi,
using TPS 62122 quite a while in an application, where
VIN might vary from 2V - 12V, required VOUT is 2.3 - 3.6V - or whatever VIN does deliver (pass through); current is max. 100mA.
Now we have a very cost sensitive application where we need something else, but all the bucks I find do have a min. voltage at ~4V; below it they switch off.
Is that intepreation right and how come? Why don't they just bypass if VIN gets below programmed VOUT?
And: most important, do you have a hint which buck I could look at?
thx. a lot