Other Parts Discussed in Thread: LMR16006,
Hi,
So far I used a LMR16006 buck converter for voltage regulation. The input voltage can vary pretty fast in between
+48VDC up to +57VDC (motor control, recuperation) and I want to replace it with a new buck converter IC,
that can handle up to +100VDC.
In the datasheet of the LMR16006 is stated, that it works for an unregulated source and automotive, so this is really for a harsh environment
and I need something similar. Can I replace the LMR16006 with a LM5163 for a motor control application with unregulated source
or should I better choose another buck converter IC?