Hi Team,
I am designing a buck converter with TPS7H4010.
In the datasheet, it is mentioned the VCC pin should not be loaded.
I want to run the device in constant frequency. So I need to pull the SYNC/MODE pin high.
The maximum recommended voltage at the SYNC/MODE pin is 5.5V.
1). TPS7H4010 is the only power supply in the system. So can I connect VCC to SYNC/MODE pin?.
My required output voltage is 3.6V and my input is 20V.
The maximum load current is less than 500mA.
The value of Rfbt is taken as 100K and the calculated value for Rfbb is 38.78K.
The inductor value is chosen to be 4.7uH and the Cout is nearly 100uF.
2) Is my calculation correct?.
3). What should be the value of the feed-forward capacitor in my design?.
4). Also, How to calculate a proper value for Cff?.
5). Is it ok to let the PGOOD pin floating?.
6). What is the maximum output current if internal LDO?.
7). The BIAS pin is connected from the 3.6V out.