Other Parts Discussed in Thread: BQ24610
Hello,
I am using the BQ24610 EVM board to charge a 4S Li-Ion battery (16.8V peak). I replaced resistors R25 and R28 on the board with a 700kOhms and 100kOhms respectively to get a high side voltage of 16.8V following the design equation VBATT = 2.1 *(1 + R25/R28). However, when I run my system in OC mode with TS and CEN both appropriately set as followed on the user guide, I am only getting a voltage of approximately 6V on the high side of VBATT with respect to ground. I am aware the design equation derives from a voltage divider with a Vfb regulated voltage of 2.1V. Vfb = Vhigh*(R28/(R28+R25) or 2.1 = Vhigh * (R28/(R28+R25)). I measured the voltage at TP13 (Vfb) with CEN on and PG status high on the board and got approximately 2.1 V, so it seems that the regulation circuit is working correctly from the output of the IC. I removed the resistors from the board then measured the resistance and both resistors had the correct impedance (they are spec'd to 1/8W which is higher than the resistors listed on the BOM at 1/10W ), so I don't think its a power issue. I put the resistors back onto the board appropriately. I measured the impedance from the GND solder connection of R28 to the - side battery input header on the board and got 0.1 Ohms (maybe resolution error). I measured the impedance from TP13 (Vfb pin) connection to the Vfb solder node of R28 and got 0.1 ohms. I measured the impedance from TP13 (Vfb pin) connection to the Vfb solder node of R25 and got 0.1 ohms. I removed C22 from the board incase i was getting a short through the dielectric of the capacitor, this did not fix my issue. I measured the resistance from TP10 to TP11 across the 0 ohms resistor and got 0.1 ohms. VBAT to PGND is OL. I can remove other capacitors from the node, but I am pessimistic that any of these capacitors would be the root of my issue.
My question is, are there any known problems with the board in the past that could cause an improper VBATT setting that do not involve resistors R25/R28? I do not think there are any issues with the solder connections or cracks/breaks in the trace that are changing the impedance.
Thank you for your time and consideration.