If we need to scale the input voltage to some of the mon inputs of the UCD90120A, is there a resistance range that is recommended for the voltage divider?
Looking at the specs for the analog inputs, the input impedance is listed a 8 Mohm min. But there is also an Input Offset Current spec of -5uA to +5 uA. Does this offset spec represent how much current the input may draw from the sensed voltage source? If so, the resistor divider on the input should be sized such that this current does not impact the divided voltage, like 500 uA. Is this correct?