Hello team,
TPS543C20A requires E48 series resistors for some pin configuration. And 1% or better accuracy is recommended in datasheet.
When customer needs to use E12 series resistor they have to make the required resistance with combination of E12 resistors.
In this case, customer can make similar resistance value to E48 value though it will require multiple resistors with high accuracy, but not the same.
Does the part require pinpoint resistance such as E48 value with 1% error? or there maybe some more tolerance in actual?
Best regards,