Other Parts Discussed in Thread: TPS25750
The datasheet of BQ25790 points out, that the IC supports USB power delivery standard and also an auto detection of the attached power supply.
USB PD standard only covers supplies with 5V, 12V and 20V output.
Therefore my question is, what happens when I connect it to a power supply able to deliver 27W max but only 9V maximum (e.g. 5V/3A and 9V/3A) but no 12V output.
Can I use the maximum output power of 9V 3A with the unit, or will I only have 5V availiable, because 9V is non-standard USB PD voltage?
Thanks in advance!