Other Parts Discussed in Thread: TPS61500
Dear Sirs and Madams,
our customer like to change the display type in his system, so I have to check the feasibility. I would appreciate your help: is that possible to drive the backlight with 21V and 160mA load current from 3,3V input? Please check the attached picture with display backlight requirements. I my breadboard setup a achieve only 110mA at 19V bei 100% PWM circle, I also can't find those limitations in the datasheet.
Best Regards
Vitali