Other Parts Discussed in Thread: TPS65130, TPS54531
One customer was develop TPS65131+α board.
When these board evaluated, TPS65131 Vout ripple were large variated.
Please see test results below, Vout ripple become 72.9mV to 887mV depend on the board.
(The same circuit, layout, and condition)
・Example Vout ripple waveform on large Vout ripple board (200mV/div and 500μs/div scale)
・Example Vout ripple waveform on normal Vout ripple board (20mV/div and 50μs/div scale)
【Question】
Please let me know about four points below;
・I think that the reason is variation of TPS65131's control circuit and external components, correct?
・If correct, is there improve point of reduce variation on external components?
・I found below E2E thread for TPS65130, is TPS65131 also possibility for depend on marking?
・If there the other reason, please let me know.
【Additional Information】
・TPS65131's spec: 5Vin to ±15V, less than 100mA
External components is, L: 4.7μH, Cout: 10μF ×3, the other parts are based on datasheet recommendation.
・When increase Iout, Vout ripple was decreased. but deference between board ripple are staying.
・5Vin side is supplied from TPS54531's 5Vout, and these ripple are depend on board, too.
But TPS54531 have not reason because when TPS54531 and TPS65131 cutoff and evaluate separately, TPS54531 was not occur large Vout ripple.
If need more detailed information, please communicate on direct e-mail.
Best regards,
Satoshi