This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62067-Q1: the max load current capability

Part Number: TPS62067-Q1

Dear team,

My customer test IL( inductor current) of 62067, and they find there is a current pulse(max 2.4A) as below, but our device has no load when testing below waveform. Could you please help analyze why the inductor current is so large under no load condition?

In addition, my customer wants to test our load current capability, so they added the 2A electronic load to 62067 with CC mode, and the power up our device, but our device has no output. Only when they decrease the current of electronic load to 0.8A, our device begins to have the 3.3V output voltage. Could you please help analyze this phenomenon?

Thanks & Best Regards,

Sherry