On the datasheet, page 1 and 2 specify Vout max as 5.7V. On page 1 it specifically states "The TPS7A90 output is adjustable with external resistors from 0.8 V to 5.7 V."
However, on section 8.1.1 (page 17), it states "the output voltage of the TPS7A9001 can be adjusted from 0.8 V to 5.2 V by using a resistor divider network." - here it's 5.2V and not 5.7V.
I'm trying to use TPS7A9001 in a design and please let me know if output of this regulator can be set up to 5.7V using a resistor divider network.
Thanks.