Other Parts Discussed in Thread: TPS54202H
Hi,
I have created a PCB using the TMS320F28377D microcontroller. I have a buck switch regulator stepping down from >8V to 7V, then going to 3 different linear voltage regulators, where one of the outputs goes to the power circuit for the MCU. When I remove the connection between the regulator to the MCU power circuit, the power seems fine. But when I reestablish the connection and power on the MCU, there is suddenly a clear sinusoidal signal at 269kHz on the power lines. It affects everything, before and after the buck regulator as well as the linear regulators.
What might be causing this, and how should I go about fixing it? It affects the output of my op amp circuits on the board.
Thank you,
Dyon