Hello,
I have a 28V DC input DC/DC converter. It is 500khz and 7V out. I must to input filter (DM and CM). Can you help me? For example a schematic etc.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a 28V DC input DC/DC converter. It is 500khz and 7V out. I must to input filter (DM and CM). Can you help me? For example a schematic etc.
Hi Emre,
The datasheet includes a detailed design procedure section that can be used to select values for TPS5430 (Section 8.2.1.2). Also, you can create a custom design with WEBENCH Power Designer which can be found at the bottom of the product folder of device (link). For example, see image below of WEBENCH design values for a 28Vin to 7Vout with a 3A output.
Regards,
Alejandro