This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ29700EVM-610:

Part Number: BQ29700EVM-610

I am testing eval kit for normal operation. 

Connected battery 3.6V  checked  for Dout / Cout and V- signal amplitudes.

Cout is ~3.4V

V- = ~2.8 (supposedly should be close to 0)

and Dout remains low 

it seems like it is detecting a load short?

NOT able to figure what is causing  Dout to stay low -- I checked everything and all looks normal as expected?

PAck+/Pack- voltage is less than 1 volt and not stable?

I have noted the swap of DOUT and V- on the silk screen for this version and have taken into account for evaluation.

Is it possible to talk to somebody?, I am located in San Jose california.

Thanks,

Yogendra