Hi,
My customer requests the dropout voltage on TLV758P under the following condition.
- Case: Vin = 1.8V, Vout = 1.35V, Iout = 300mA
Please advise us.
Thanks and best regards,
M.HATTORI.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer requests the dropout voltage on TLV758P under the following condition.
Please advise us.
Thanks and best regards,
M.HATTORI.
Hey Hattori,
From the EC Table:
For Vout=1.35 and using the worst case of Vdo=400mV @500mA
Then Rds=800mOhms
For Vout=1.35V @ 300mA then Vdo=240mV.
Your Vin must be within 1.59V. Therefore, using 1.8V would give you 450mV of headroom.
Best,
Edgar Acosta