Design the circuit according to Webench:Vin=11-13V、Vout=0.82V、Iout=20A
Ripple noise = 200mVp-p, which is very large.
The SW frequency is also unstable.
The actual load is about 1 to 5A, but there is no change in ripple noise.
Also, Vout = 0.85V, which uses the same IC, is more stable.
Are there any possible causes and countermeasures?
Figure 1:Ripple Waveform
Figure2:Figure1 Zoom
Figure3:SW Waveform