Customer is using 1550 rechargeable lithium battery with TPS61094 in Automatic Buck or Boost mode. Nominal battery voltage is 4V.
Vin = 5.1V
Vout = 3.3V
Vchg = 4.1V
Ichg = 100 mA
It appears to me the the super cap voltage must be less than the Vout for the device to operate properly. Is that correct?
Please advise.
Thanks,
Mark