Hello,
1- I have a bq76PL455EVM. It connects with microcontroller. At the first power-up, the D22 led seems to turn on as soon as the Wake signal is gone, but it flickers and the EVM does not wake up. I connect BAT16 and BAT0 before Vsense inputs. Since I use a single structure, I feed the VP pin from the microcontroller. But in no way does the EVM wake up. When I look at the Wakeup test point with the oscilloscope, I see that it suddenly drops from 5V to 2V.
2- By the way, I am testing for 6 cells and the led of the last cell is constantly on, even though there is no power.
What could be the problem, can you help?