Do you have value for the time between EN pin becoming active until Vout becoming active?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do you have value for the time between EN pin becoming active until Vout becoming active?
Thanks.
Hello Fraser,
Would the EN pin be tied to VIN or is VIN already stabilized when EN is activated?
Best,
Juliette
Hi Fraser,
Your start-up time will be influenced by your soft-start value capacitor.
Would you be able to link the schematic you are using so we can verify Ton?
Bets,
Juliette
Hi Fraser,
Thank you for sharing your schematic with us. I will go ahead into the lab to show you real data. Please give me a day so I can collect the data.
On the meanwhile, from simulations I obtained the following:
The red is Ven and blue is Vout. From the point where EN is completely high to Vout completely high ~146us
From EN high to 90% of VOUT the time shows 131us.
Best,
Edgar Acosta
Thanks, Edgar.
It looks promising, since we require that it goes high in less than 100ms in our application.
Hey Fraser,
No problem. I am currently working on this. I will update later today.
Best,
Edgar Acosta
Hello Fraser,
Here are the Scope Shots I collected today:
Vin=5.8V
Vout=5.1V
Ven=5.8V just to set a value, but Vin is not tied to Ven.
As observed timing~1.3ms.
Best,
Edgar Acosta