Hi
i have an issue when make a power board with TPS63031DSKR
When i turn off , it still have 0.5V at output ( while turn on is 3.3V is OK)
Power from battery 4.2V , 2000mah
Please help to solve this issue.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alone,
Could you help to capture waveform of PIN Vin EN and output during this issue?
Regards
Tao
Hi
im sorry for delay for sending waveform
As you seen, when EN pin low, output have still 0.5V
when high, output have 3.3V.
Please send me message , i will help to send you full my design schematic to review
Thanks.
Hi alone,
I have an email sent to you, please check it.
Hi Zuan,
Let us keep in touch via email. This reply is to indicate that the introduction of the problem, please do not reply. Thanks
Regards
Tao